2026-05-10 8:15 AM
As in attached image, the build hammer icon is greyed out after importing project made in STM32CubeMX version -- 6.17.0 to CubeIDE version -- 2.1.1.
I have selected tool chain as STM32CubeIDE in the Project Manager in CubeMX and after generating the code, i tried by opening the project from CubeMX as well as importing project to CubeIDE.
MCU : STM32G474 series.
Thanks for the help in advance.
2026-05-11 1:54 AM
Hello @KishanMalanthra
It seems that the project has not been imported properly.
It's recommended that you check this post: Solved: Can't build imported demo project - STMicroelectronics Community and follow the steps to import your project into CubeIDE.
KR, Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.