2024-03-14 1:49 PM
Hi all,
This is a bit silly but it is annoying to me. The picture below shows an empty project (top: DiscoBaseEmpty) and one cubeIDE project (bottom: DiscoBaseIDE) for a dual core STM32H745 disco board. I'm learning what's required to get an empty project to work. I recreated the folders structure of the cubeIDE project with the files and folders in the empty projects. The DiscoBaseEmpty_CM4 is compiling without errors. Although, I only added HAL_Init() to main() for now.
The Core folders (in both projects) have 3 other subfolders (Inc, Src and Startup) . The cubeIDE projects shows them too but in the empty project cubeIDE seems to insist in placing "shortcut" folders (Core/Src and Core/Startup) and I can not get rid of them. Trying to delete them ask if I really wanna delete them from the filesystem which is not what I want. I want to get rid of the shortcut folders... and why does it do it for the empty project and not the one created as cubeIDE? Thanks.
Solved! Go to Solution.
2024-03-15 11:56 AM
I found how to remove the shortcut folders. when I was adding the folders to the CM7 core project. It looks like I added them as "/DiscoBaseEmpty_CM4/Core/Src" and "/DiscoBaseEmpty_CM4/Core/Startup" to the source locations in the project properties (project properties -> C/C++ general -> Paths and Symbols -> Source Location Tab).
I removed the two entries and added "/DiscoBaseEmpty_CM4/Core". This automatically removed the shortcut folders and the project still compiled without errors.
2024-03-15 11:56 AM
I found how to remove the shortcut folders. when I was adding the folders to the CM7 core project. It looks like I added them as "/DiscoBaseEmpty_CM4/Core/Src" and "/DiscoBaseEmpty_CM4/Core/Startup" to the source locations in the project properties (project properties -> C/C++ general -> Paths and Symbols -> Source Location Tab).
I removed the two entries and added "/DiscoBaseEmpty_CM4/Core". This automatically removed the shortcut folders and the project still compiled without errors.