cancel
Showing results for 
Search instead for 
Did you mean: 

Why do I get error when I build project?

PStur
Associate

0690X000009YD3CQAW.png

Hello,

Why do I get error when I build project?

I have imported the project

Can anyone help me if I send the project files?

With Kind regards / Peter

16:12:11 **** Build of configuration Debug for project test ****

make all

C:\Program: C:\Program: Permission denied

make: *** [Src/bldc.o] Error 126

"make all" terminated with exit code 2. Build might be incomplete.

16:12:16 Build Failed. 1 errors, 0 warnings. (took 4s.534ms)

2 REPLIES 2
PStur
Associate

Here is the project that I have problems with

Markus GIRDLAND
ST Employee

Where did you find the project? Was it created for STM32CubeIDE to begin with or some other IDE?