Skip to main content
RLee.2
Associate
February 18, 2020
Question

Undefined reference to 'osThreadJoin'

  • February 18, 2020
  • 3 replies
  • 2091 views

Hi forum,

I'm developing using the STM32CubeIDE on the NUCLEO-F746ZG board running FreeRTOS. In the process of developing my application that makes heavy use of OS constructs, I've run into a missing/unimplemented function problem, namely osThreadJoin. The function is declared in cmsis_os2.h, but not defined in cmsis_os2.c, with all the other OS functions. How can I get access to this function?

Thanks,

Richard

This topic has been closed for replies.

3 replies

JBaco.1
Visitor II
September 16, 2020

Hi all,

Same problem here. Anyone as a solution ?

Thanks.

Julien

SGeof.1
Visitor II
March 24, 2022

Hi,

Did you guys figure out a solution?

Thanks,

Sam

ZDima
Associate
September 5, 2022

After hour of search found this on github.com:

/ARM-software/CMSIS-FreeRTOS/blob/9cf2e4b4f621abfed0ee2de421d31988f8b1b0f6/DoxyGen/General/src/cmsis_freertos.txt#L733

Thread Management:

- osThreadDetach: \token{not implemented}

- osThreadEnumerate: supported

- osThreadExit: supported

- osThreadGetCount: supported

- osThreadGetId: supported

- osThreadGetName: supported

- osThreadGetPriority: supported

- osThreadGetStackSize: \token{not implemented}

- osThreadGetStackSpace: supported

- osThreadGetState: supported

- osThreadJoin: \token{not implemented}

- osThreadNew: supported

- osThreadResume: supported

- osThreadSetPriority: supported

- osThreadSuspend: supported

- osThreadTerminate: supported

- osThreadYield: supported

Also in the same document:

- osThreadDetach, osThreadJoin() and attribute osThreadJoinable are not supported (osThreadNew returns NULL when osThreadJoinable attribute is specified).

It would be nice if this information was clearly stated in documentation (?) and in the headers.