cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to write to microcontroller with stlink-v3minie

baby_chicken
Senior

When I try to write to stm32h742vgt6 using stlink-v3minie, Target is not responding, retrying... and cannot write.

The same microcontroller can be written to the board on which it is mounted. In the same program.

What are the possible outcomes in this case?
Is it just a bad solder or something else, or can you give me a few possibilities?
Thank you in advance.

 

symptoms↓

Failed to reset target.

Target is not responding, retrying...

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Target is not responding, retrying...

Shutting down...

Exit.

 

1 ACCEPTED SOLUTION

Accepted Solutions

Sorry for the late reply.

 

After much investigation, I found that pin 63 of the microcontroller was conducting with 5V due to a design error.

 

 

View solution in original post

5 REPLIES 5
Andrew Neil
Super User

@baby_chicken wrote:

When I try to write to stm32h742vgt6 using stlink-v3minie,


Show your connections.

 


@baby_chicken wrote:

The same microcontroller can be written to the board on which it is mounted.


What do you mean by that?

What board is it?

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

This is a home-made board using stm32h742vgt6.
It is not NUCLEO etc.
Best regards.

Show the schematic of the board.

What do you mean by, "The same microcontroller can be written to the board on which it is mounted" ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Sorry for the late reply.

 

After much investigation, I found that pin 63 of the microcontroller was conducting with 5V due to a design error.

 

 


@baby_chicken wrote:

I found that pin 63 of the microcontroller was conducting with 5V due to a design error.


Hence why it's important to show the schematic of the board!

Has that fixed the problem?

If so, please mark it as the solution.

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.