cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to start motor with MC sdk generated code

madhavP
Associate II

hi,

I have been trying to run PMSM motors with B-G431B-ESC1, I follow the steps given in the user manual,

1. I profile the motor and save the parameters

2. use the motor control workbench to generate a project, and generate source code,

3. run it in Cube IDE to flash it on the development board.

However, I am unable to run my motor with that source code. The motor doesn't even start. I also face inconsistency when running the motor with the same source code on different occasions. What could be the issue, and what should I do to resolve this issue?

since the profiler is working, where can I get a profiler code based on which the profiling .hex file is created to debug the issue?

Thank you,

Madhav

0 REPLIES 0