cancel
Showing results for 
Search instead for 
Did you mean: 

TM32CubeIDE 1.13.1 and Nucleo-F429ZI - Linker Error

jens3
Associate

Hello,

when I create a new project with Ide 1.13.1 and Nucleo-F429ZI and enable ETH,  LWIP and HTTPD then I get following linker errors. Seems some module are not compiled automatically. What could be the reason? How to solve?

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./LWIP/App/lwip.o: in function `MX_LWIP_Init':

C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/App/lwip.c:63: undefined reference to `lwip_init'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/App/lwip.c:71: undefined reference to `netif_add'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/App/lwip.c:74: undefined reference to `netif_set_default'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/App/lwip.c:79: undefined reference to `netif_set_up'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/App/lwip.c:84: undefined reference to `netif_set_down'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/App/lwip.c:88: undefined reference to `netif_set_link_callback'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/App/lwip.c:93: undefined reference to `dhcp_start'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/App/lwip.c:98: undefined reference to `ethernet_input'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./LWIP/Target/ethernetif.o: in function `low_level_init':

C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:175: undefined reference to `memp_init_pool'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./LWIP/Target/ethernetif.o: in function `ethernetif_init':

C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:404: undefined reference to `etharp_output'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./LWIP/Target/ethernetif.o: in function `pbuf_free_custom':

C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:414: undefined reference to `memp_free_pool'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./LWIP/Target/ethernetif.o: in function `ethernet_link_check_state':

C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:635: undefined reference to `netif_set_down'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:636: undefined reference to `netif_set_link_down'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:674: undefined reference to `netif_set_up'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:675: undefined reference to `netif_set_link_up'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: ./LWIP/Target/ethernetif.o: in function `HAL_ETH_RxAllocateCallback':

C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:684: undefined reference to `memp_malloc_pool'

C:/ST/STM32CubeIDE_1.5.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.11.3.rel1.win32_1.1.0.202305231506/tools/bin/../lib/gcc/arm-none-eabi/11.3.1/../../../../arm-none-eabi/bin/ld.exe: C:/IMT2021/Stm32WorkspaceTest2/Test230803/Debug/../LWIP/Target/ethernetif.c:693: undefined reference to `pbuf_alloced_custom'

collect2.exe: error: ld returned 1 exit status

make: *** [makefile:67: Test230803.elf] Error 1

"make -j8 all" terminated with exit code 2. Build might be incomplete.

 

2 REPLIES 2
Imen.D
ST Employee

Hello @jens3 ,

Check your defined functions and libraries.

 Take a look at this article: How to create project for STM32H7 with Ethernet an... - STMicroelectronics Community

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

"Check your defined functions and libraries." -> Unfortunately I don't understand your hint. I have nothing defined manually. I enabled in CubeIde 13.1  ETH, LWIP and HTTPD only.

With best regards,

Jens