2023-08-28 2:37 AM
Hello, I'm trying to implement Low power sleep on STM32WB. The sequence is as per LPSLEEP example:
HAL_PWREx_EnableFlashPowerDown(PWR_FLASHPD_LPSLEEP);
SystemClock_Decrease(); //MSI 2MHZ
HAL_SuspendTick();
HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI);
//... Sleep until wake on interrupt (EXTI15_10_IRQn)In my case CPU1 never sleeps, or it wakes straight away. I've tried disabling the other interrupts with HAL_NVIC_DisableIRQ(), __disable_irq(), no success.
What could be causing it? CPU2 and BLE stack are running, what needs to be done on this side? Thanks
2023-08-28 8:26 AM - edited 2023-08-28 8:27 AM
Hello @MHast.11.
Thank you for posting.
I suggest that you consult this PDF AN5071 which describes the Power Modes features of the STM32WB Series.
You can also take a look to the examples available under https://rb.gy/nw2hb .
Thank you.
Mahmoud.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.