2024-07-01 07:49 AM
When i try to create a STM32 project on Cubeide (wayland) i've been getting this error and can't select any board. I can't even see the Window to select board/mcu etc.
I've also tried to use it with Xorg and it's worse. The application crashes after a few seconds of pushing create stm32 project.
I've checked 14.0, 15.0 and 15.1 none of them working. Is stm32cubeide for linux broken?
2024-07-15 06:39 PM
I'm getting the same problem on Window10.
This is at the top of the screen
And as you can see below, there are no boards to be selected from.
If I go back to the select by MCU/MPU instead of by board and already know what specific board I want, I can then click on the board as an option.
Also this only happens when I try to start a new project from inside STM32CubeIDE. When I open CubeMX directly, the board selection tool works properly.
I know the work around for this, but is there a fix, what should I be reloading?