cancel
Showing results for 
Search instead for 
Did you mean: 

SWV not working with STM32CubeIDE

thejc
Associate II

Serial wire viewer is not showing since STM32CubeIDE version 1.0.1. It has worked before in version 1.0.0.

I'm trying to use it with a STM32F103RBT6 but also tried it with a Nucleo F103RB.

The live Expressions work perfectly fine, but not the SWV it just does nothing (no I havent forgot to press the record button).

0690X000009YQRbQAO.jpg0690X000009YQRMQA4.jpg

3 REPLIES 3

Don't you have to enable some ports?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hansd56
Senior II

As far as I know only CubeMX changed going from 1.0.0 to 1.0.1. Which debug probe are you using? Show as the Debugger configuration.

thejc
Associate II

I've fixed it, it was not a software problem. I just had a bad connection on the SWO pin.