2025-05-19 2:47 AM - edited 2025-05-19 2:49 AM
Hello all,
I have been hanging on to an anctient version of ubuntu for a LONG time because I need to use STM32CubeIDE,
sadly, IT required me to update because you know..... security and stuff.
I was resisting because I knew I would get this error:
Could not determine GDB version using command: arm-none-eabi-gdb --version
arm-none-eabi-gdb: error while loading shared libraries: libtinfo.so.5: cannot open shared object file: No such file or directoryAnd I had tried to install the required file before, even add a symlink to the so.6 version in the past with no luck. So today I made the update, and when I hit debug right after re-installing the Ide, i got the lovely message.
So it this it for me? Do I need to bug IT to get me a new PC simply to run an old version of ubuntu or is there some way for me to actually run this?
I am guessing no as it seems to be part of the ide...
My current version is: base: Ubuntu 24.04 noble
Anyone else have any luck with this? I read some other posts about this, but none have helped.
Thanks all!!!
2025-05-19 3:19 AM - edited 2025-05-19 3:21 AM
First, I suggest to run "ldd arm-none-eabi-gdb", which should tell you more about the actual dependency issues.
Ubuntu 24.04 is relatively recent, though.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.