cancel
Showing results for 
Search instead for 
Did you mean: 

SWV doesn't work on STM32CubeIde 1.14 for Nucleo-H743ZI2

Wojt
Associate II

Hi

I need this set up to debug harder issue I encountered. I tried to search through available post but can't find anything similar enough. In the past I used SWV on STM32F411 and it worked well so I have a bit experience.

Anyway:

-debug setup in CubeMX looks little bit different, I have chosen this:

Wojt_0-1704747438907.png

-clock is set up to 480MHz:

Wojt_1-1704747564117.png

- firmware of ST Link V3 is (I seen some posts on other problems suggesitng to downgrade, I don't know if it is a case here, moreover, I don't know how to dongrade to selected version):

Wojt_2-1704747762932.png

-debug config seems to be recognizing proper clock:

Wojt_3-1704748013597.png

-I try to set up SWV to see just uwTick, nothing happens in SWV data window when running the SW:

Wojt_4-1704748124196.png

- surprisingly sometimes, when playing with sampling setting, I see sometimes few values displayed in trace window but it hangs up anyway and is randomly working = completely useless

Wojt_5-1704748686587.png

 

Does anyone know if I am doing anything wrong or does any workaround exist?

 

Greetings

Wojt

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief II

Hi,

You set core clk to 480MHz - but in debug SWV you write 240MHz ; 

if not giving korrekt frequency , swv dont work.  So set 480, if core is at 480.

+

I choose this (its working):

AScha3_0-1704749714693.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
AScha.3
Chief II

Hi,

You set core clk to 480MHz - but in debug SWV you write 240MHz ; 

if not giving korrekt frequency , swv dont work.  So set 480, if core is at 480.

+

I choose this (its working):

AScha3_0-1704749714693.png

 

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Evangelist III

The number you give as the "Core clock" in the dialog is the value of global variable SystemCoreClock after you call SystemClock_Config() divided by a million. For example, 240000000 -> 240.0

(by the way - this is why the SWV/ITM trace won't work until SystemClock_Config returns ;)

Wojt
Associate II

Thank you for quick help!