STMCUBE IDE can we use two debug window at time?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-29 10:26 PM
Hello,
I am using the NUCLEO-h745ziq board. I am using two board for SPI loopbacking.One board as master and one board as SLAVE. Can we use the two debug window at time. Because I launch the one stmcubeIDE window 1.5.1 and another from stmcubeide 1.6.1 because i have only one drive C. When i debugging the two board, one board debugging ic completed when i try to debug second borad i get the error of GDB server failed. I am unable to undestand why it is shown .Becuase my two board independantly working when i debug it one by one.Can someone please helpme?
Solved! Go to Solution.
- Labels:
-
DEBUG
-
STM32CubeIDE
-
STM32H7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-30 6:37 AM
Hello @MDeva.1​,
Yes debugging programs with two or multiple boards is possible within STM32CubeIDE.
It can be realized using two ST-LINK or SEGGER J-Link probes at the same time. Please ensure that you are not using the same port number for both projects selected in the Debugger tab in the Debug Configurations dialog.
I recommend you to following the 3.6.3 section "Debug multiple boards" of the UM2609 STM32CubeIDE user guide.
Chahinez.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-29 11:44 PM
Hi,
I believe the issue is that both GDB servers are using the same port (usually it is port 61234). You should try to change the "Debug configuration" -> "Debugger" -> "GDB port" for one of the 2 IDE instances (I'm not using CubeIDE, so I can't help precisely here), and maybe also specify the ST-Link serial number to use for each debug instance, so the IDE knows which debugger to use.
See the picture below for Atollic:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-30 6:37 AM
Hello @MDeva.1​,
Yes debugging programs with two or multiple boards is possible within STM32CubeIDE.
It can be realized using two ST-LINK or SEGGER J-Link probes at the same time. Please ensure that you are not using the same port number for both projects selected in the Debugger tab in the Debug Configurations dialog.
I recommend you to following the 3.6.3 section "Debug multiple boards" of the UM2609 STM32CubeIDE user guide.
Chahinez.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-31 11:47 AM - edited ‎2024-07-31 11:47 AM
Don't forget to change the ports on your RTOS Kernel Awareness and Serial Wire Viewer if you're using them.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-04-21 5:59 PM - edited ‎2025-04-21 6:19 PM
Just for your information.
The chapter number 3.6.3 Debug multiple boards mentioned by ChahinezC is now chapter 3.1.6.3 Debug multiple boards of user manual UM2609 as of today, April-22-2025.
Menu of STM32CubeIDE is also slightly changed on STM32CubeIDE 1.18.0.
Select Run > Run Configurations... , and you can find Run Configuraions window.