cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5G9VJT6Q not supported?

Ricko
Senior III

Hi,

I just tried selecting the STM32U5G9VJT6Q in CubeIDE and the "Next" button to start a project based on it is not enabled and there is a note at the top of the window saying it is not supported (see attached screenshot)?

I assume that is incorrect and I perhaps need to download some additional data somehow (I didn't for other micros though)?

Thank you

 

Amz 001530.jpg

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Ricko 

I'm not able to reproduce this behavior using CubeMX 6.12.1 and CubeIDE 1.16.1:

STTwo32_0-1730217164586.png

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @Ricko 

I'm not able to reproduce this behavior using CubeMX 6.12.1 and CubeIDE 1.16.1:

STTwo32_0-1730217164586.png

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STTwo-32
ST Employee

Have you solved your issue. If no, please add more details.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.