2024-05-03 12:18 AM - edited 2024-05-03 12:23 AM
With the STM32CubeIDE I can't debug a firmware, as always the connection is lost:
Download verified successfully
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Target is not responding, retrying...
Shutting down...
Exit.
Any ideas?
kind regards
Johannes
Solved! Go to Solution.
2024-05-03 01:46 AM - edited 2024-05-03 04:42 AM
Hello @johannes-lichtenberger and welcome to the ST Community 😊.
I suggest you take a look at this Post. It should be helpful.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-03 01:42 AM
Tell us your hardware? Some commercial board or something you build? Check and test other cables and USB ports. Check wiring. Check your setup.
2024-05-03 01:46 AM - edited 2024-05-03 04:42 AM
Hello @johannes-lichtenberger and welcome to the ST Community 😊.
I suggest you take a look at this Post. It should be helpful.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-03 06:29 AM
I've checked using other USB-Ports, but it didn't help. I'm going to check another USB 3 to USB-C cable, but I doubt, that it helps, either. The board is a new STM32U083C-DK.
kind regards
Johannes
2024-05-03 09:46 AM
Double check with STM32 Cube Programmer.
Any details on the ST-LINK/V2EC model used here?
2024-05-06 07:06 AM
Thanks, I've enabled the debugging PINs in the Cube / meaning removing them from the unused PINs... so, now it seems it's possible to debug without problems... 🙂
Thanks
kind regards
Johannes