cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L524 SDMMC error reported incorrect

Sid Price
Senior

If a timeout occurs from "SDMMC_CmdOpCondition" (error #4) the calling function, "MMC_PowerON", returns "HAL_MMC_ERROR_UNSUPPORTED_FEATURE".

Is this correct?

Sid

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
CNhan.1
Associate

I had the same issue as you, I don't understand why there is no suggestion from ST for this topic yet.

That's how forums often work, ST doesn't have a heavy presence here, and you're reliant of others with the same combination of hardware or ability to debug/diagnose.

Might be card specific, or a board related.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MTriv.1
Associate II

I have the same issue in STM32L476G when trying an eMMC connected via microSD to eMMC adapter. Were you able to find a fix for this problem?

Rtomy.1
Associate II

Did anyone solved this? I am having the same issue in my custom board.

jerry_sandc
Associate III

I have same error occuring in the initialization code on my STM32F769-EVAL board!  :thinking_face:

I do have the SD card that came with the eval board plugged in properly.  Maybe there's some jumper setting, i'll check it out.

I just looked at the eval board manual.  Looks like I have to make some solder modification and change a jumper to allow the SD cards to work, since some pins are shared with the camera.  You might have the same issue.