2026-01-12 3:55 PM
CubeMX 6.16.1
MacOS 15.7.3
STM32F469NIHX
Multimedia - DSIHOST - Data and Clock Lanes - click,click,click
Show Advanced Parameters - check
HS Transmission fine tuning and LP Transmission fine tuning
Transmission Delay on Clock Lane and Transmission Delay on Data Lanes
These items refer to 2-bit wide fields in DSI_WPCR1 but CubeMX allows values from 0-10, which would be 3.32-bits wide. By setting the clock transmission delay to, say, 10, the data clock delay gets overwritten as well. Data delay overwrites the low power clock delay, and so on.
The actual data range for these items should be [0,3], and HAL_DSI_SetSlewRateAndDelayTuning should probably sanitize the parameter Value before using it.
Solved! Go to Solution.
2026-02-25 2:53 AM
Hello @Andrei Chichak
This issue has been resolved in the latest version of STM32CubeMX 6.17.0
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-12 11:04 PM - edited 2026-01-13 3:44 AM
Hello @Andrei Chichak
Your detailed explanation is much appreciated.
Issue has been escalated to dev team for resolution under internal ticket ID 225025
I will keep you posted with updates;
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-25 2:53 AM
Hello @Andrei Chichak
This issue has been resolved in the latest version of STM32CubeMX 6.17.0
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.