cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H745ZI Dual Core Controller

Embrill_Nishant
Associate

How to flash the dual core controller(STM32H745ZI) blinky code using either of stm32loader and etc platform anyone knows?

2 REPLIES 2
FBL
ST Employee

Hi @Embrill_Nishant 

Try the following example

STM32CubeH7/Projects/NUCLEO-H745ZI-Q/Examples/GPIO/GPIO_EXTI at master · STMicroelectronics/STM32CubeH7 (github.com)

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I don't want to use MPU; I just want to know if it's possible to load a bin file onto the dual-core controller using stm32loader (a Python-based loader for loading bin files into the controller) or stm32cubeprogrammmer.
One more thing , when I try to run a simple example in STM32CubeIDE, such as controlling three LEDs where the first LED is controlled by the M4 core and the second LED by the M7 core, I encounter a hard fault error. I'm unsure why this error is occurring. I have shows the error in below.....

break the address.png