cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h7 ethernet configration

rockey1
Associate

how i am config ethernet in the stm32h753xi6 board ?

22 REPLIES 22
Andrew Neil
Super User

@rockey1 wrote:

 the stm32h753xi6 board ?


Which stm32h753xi6 board ?

stm32h753xi6 is just a chip part number - it doesn't identify a board.

 

Have you searched the Knowledge Base ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
ST Employee

Hello @rockey1 and welcome to the ST community,

As said by @Andrew Neil stm32h753xi6 is a chip not a board!

Are you talking about STM32H753_EVAL that contains a STM32H753XIHx? or it's a custom board?

For the Eval board you can inspire from the examples which are provided in the Cube package using LWIP: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Applications/LwIP

or by referring to this article: How to create a project for STM32H7 with Ethernet and LwIP stack working

For custom board you need to have the PHY driver.

Hope that helps.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

sorry my mistake i am talking about on stm32h753 chip 

 

That answer doesn't help much ..

@rockey1 wrote:

sorry my mistake i am talking about on stm32h753 chip 


Ethernet is not UART or SPI, it's a set of complex hardware and software staff.

So what hardware are you using? and what Ethernet stack you will be using?

Did you check my previous comment?


To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@rockey1 wrote:

sorry my mistake i am talking about on stm32h753 chip 


That's not even a chip - that covers a whole family of chips!

 

AndrewNeil_1-1751472257395.png

 

You can't do anything with just a chip - it needs to be on a board, with a few other components.

So the question is, what board do you have?

  • If it's an ST board, just give the full name
  • If it's a custom board, you'll need to give full details.

Please See: How to write your question to maximize your chances to find a solution.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

An STM32H753XI6 microcontroller mounted on a specially made PCB with an Ethernet interface is what I'm working with. I've given the STM32 board an IP address and connected it to a PC via an Ethernet cable. I can't, however, successfully ping the STM32 from the PC.

I need instructions on how to set up the STM32H753XI6's Ethernet peripheral correctly and how to put the required code into place to enable Ethernet communication. I specifically need help with:

Setting up the PHY and Ethernet hardware

Configuring a static IP address

Putting into practice fundamental network functions (like answering a ping)

I would be very grateful for any guidance or sample code that could help me set up Ethernet communication on this microcontroller.


@rockey1 wrote:

An STM32H753XI6 microcontroller mounted on a specially made PCB with an Ethernet interface is what I'm working with.


So, as described in How to write your question to maximize your chances to find a solution, You need to provide the schematics for that board.

There is no other way that we can know what you're working with!

 


@rockey1 wrote:

 I specifically need help with: Setting up the PHY and Ethernet hardware


Then, obviously, you will need to tell what PHY you are using, and how it is connected to the STM32.

That's why you need to provide schematics for your board.

 


@rockey1 wrote:

I would be very grateful for any guidance or sample code that could help me set up Ethernet communication on this microcontroller.


Have you looked at the links I provided earlier?

Have you looked at the links @mƎALLEm provided earlier?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

all link are okey and i am useing phy layer LAN8742 can you help me how to configure eternet in stm32cubeide and what code are write in stm32 cube ide.

 

@rockey1 

Did you already open and read the links we provide? especially How to create a project for STM32H7 with Ethernet and LwIP stack working ??

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.