cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h7 ethernet configration

rockey1
Associate II

how i am config ethernet in the stm32h753xi6 board ?

23 REPLIES 23

yes i have already use that link and my eternet also not working 

 

"not working" could not help others to understand your issue.

1- What kind of issue? you need to describe it. 

2- What did you try at this stage in term of debug?

3- You need to provide more and more details:

  • Your board schematic
  • Your project.

@STackPointer64 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
STackPointer64
ST Employee

@rockey1 

Could you please provide your STM32CubeMX configuration file (.ioc) so I can verify your setup? Additionally, if possible, please share your schematics and project files. This will help me pinpoint the root cause of the issue and guide you toward a solution.

To improve visibility of answered topics, please click 'Accept as Solution' on the reply that resolved your issue or answered your question.

Screenshot 2025-07-03 161748.pngScreenshot 2025-07-03 161829.pngScreenshot 2025-07-03 161920.pngScreenshot 2025-07-03 162000.pngScreenshot 2025-07-03 162027.pngScreenshot 2025-07-03 162125.pngScreenshot 2025-07-03 162241.pngScreenshot 2025-07-03 162305.pngScreenshot 2025-07-03 162330.pngScreenshot 2025-07-03 162422.png

this config and code i am using to run eternet in my stm32h753xi6 chip i am getting this output when i am ping ipScreenshot 2025-07-03 163025.png

can you please help me how i am config and what code i am use to successful run eternet in the stm32h753xi6 chip.

@rockey1 

Ethernet is not about Software but also about the Hardware. You need to post:

1- Your schematic

2- Your project. If it's not possible to share it in public please share it in private with @STackPointer64 

Thank you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
rockey1
Associate II

i need a conection between my pc or stm32h753xi6 chip or ping that stm 32 ip and response that is ping that i want only.


@rockey1 wrote:

can you please help me 


Not if you don't provide the information requested!

As @mƎALLEm said, you need to provide:

1- Your schematic;

2- Your project. 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

i have not access schematic  or project which company i have doing work that company given me task to run eternet on the board.