2021-12-20 03:14 AM
So I recently purchased an STM32F768I-DISCO board and every time I try to run or debug a code, I get "The selection cannot be launched, and there are no recent launches�?. I do not get any build errors so it I believe it has something to do with the configuration of ST-Link or maybe the board is faulty. Could someone help me out here? Thanks!
2021-12-20 07:16 AM
Can STM32CubeProgrammer connect and interact with the device correctly?
How did you generate the project? Did you generate through CubeMX or did you import the code? If the latter, you will need to set up a configuraiton.
2021-12-21 10:20 AM
Hi, thank you for your reply. I realised that I needed to manually select the run configurations as I am using imported code.