cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F479VI no SDRAM in CubeiDE?

PGroe.2
Associate III

Hi

I just testing some options for a future project which possibly involves a STM32F479VIT and I try to understand if it can handle an IS42S16400J-7TL SDRAM module.

So I created a test project in CubeIDE but it does not show any SDRAM option in the FMC section. But in the Datasheet of the F479 there is a whole section dedicated to SDRAM. I am missing something? It shows only SRAM and PSRAM etc...

0693W00000AOo0OQAT.png

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

The LQFP100 chip lacks some pins required for SDRAM. One option is to move up to an LQFP144.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Guru

The LQFP100 chip lacks some pins required for SDRAM. One option is to move up to an LQFP144.

If you feel a post has answered your question, please click "Accept as Solution".
PGroe.2
Associate III

Thanks, got it.