cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446RET SPI Problem With CC1120 Device

mrkayaalp
Associate III

Im currently working on a custom PCB with cc1120 as transceiver and stm32f446RET6 as MCU. I integrate the cc1120 library from IT's library. The device uses SPI as serial communication. Here is the communication example in given datasheet.

Pasted image 20240424003521.png

 With this information i configured the SPI settings as:

Pasted image 20240424003611.png

after that i use HAL_SPI_TransmitRecieve( ) function as my comm func. in driver. But im not gonna share the complex library instead i will demonstrate the situation. My CS pin and cc1120 reset pin is logic HIGH in idle by software.

txdata[0] = 0x30;

HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, 0);

HAL_SPI_TransmitReceive(&hspi1, txdata, rxdata, 1, 500);

HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, 1);

/* USER CODE END 2 */  

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while (1)

{

txdata[0] = 0x2F;

HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, 0);

HAL_SPI_TransmitReceive(&hspi1, txdata, rxdata, 1, 500);

HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, 1);

HAL_Delay(20);

txdata[0] = 0x8F;

HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, 0);

HAL_SPI_TransmitReceive(&hspi1, txdata, rxdata, 1, 500);

HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, 1);

HAL_Delay(20);

txdata[0] = 0x00;

HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, 0);

HAL_SPI_TransmitReceive(&hspi1, txdata, rxdata, 1, 500);

HAL_GPIO_WritePin(SPI1_CS_GPIO_Port, SPI1_CS_Pin, 1);

HAL_Delay(20);

/* USER CODE END WHILE */

/* USER CODE BEGIN 3 */

}

In this code first i use command SRES (0x30) for reset the device. In this situation device must be send chip status from MISO line when i start to transmit from MOSI line. But i cant see the chip status byte in MOSI line (Im seeing 0xFF as chip status byte). Chip status byte explained in datasheet as: "When the header byte, data byte, or command strobe is sent on the SPI interface, the chip status byte is sent by the CC112X on the SO pin." and:

Pasted image 20240424004458.png

Then in while loop , want to access PART NUMBER register for read the chip id. The chip id reg is a extended register (0x2F8F). So first im transmitting 0x2F then 0x8F after that i want to recieve chip id. But again i cant get anything.
So i cant reach the cc1120 device but i don't know why. I tried several different configurations. I use oscilloscope for see the lines and SCK line looks fine to me. Here is the MCU and the RF part of pcb. Almost same as the reference design of the cc1120:

Pasted image 20240424005159.png

Pasted image 20240424005211.png

So there is a external 32MHz oscillator indicated as Y2 but we don't have it so we use 32.578 MHz instead. Is that a problem for the device? Here is the scope results:

WhatsApp Görsel 2024-04-24 saat 01.13.10_a240d5a4.jpg

Ch1:SCK
CH2:MOSI
In MISO line im only seeing logic HIGH voltage and nothing else. I think that MOSI line scope results overlapping in while loop but im not sure. How can i solve this problem?

This discussion is locked. Please start a new topic to ask your question.
17 REPLIES 17

My settings are same as yours. Which library are you using for the device?

I worked from the SWRA493 (October 2015) CC112x-CC1190 Boost Software Examples:

https://www.ti.com/tool/BOOSTXL-CC1120-90#related-design-resources

https://www.ti.com/lit/an/swra493/swra493.pdf

Another advantage of starting with a manufacturer's dev kit!

Your other 2 threads have already pointed-out two flaws in your code:

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1353735/cc1120-spi-problem-with-stm32f446re-custom-pcb/5161874#5161874

and that's apart from any hardware issues on your custom board.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

At the moment, I do not have the budget to purchase a development kit. I have noticed that the SO line never goes low, which I have already pointed out in the scope results. I am wondering if there are any flaws you can identify in my design.


@mrkayaalp wrote:

I have identified an issue with my current custom PCB, 


Please be sure to update both your other threads with this key information!

 


@mrkayaalp wrote:

 I have noticed that the SO line never goes low


As previously noted, that could be due to the GND pad not properly connected:

https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1271367/cc1125-cc1125-spi---miso-so-stays-low

 


@mrkayaalp wrote:

 I am wondering if there are any flaws you can identify in my design.


That's really a question for the TI forum - nothing to do with ST.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I expressed myself incorrectly; let me edit my reply for clarity.

Probably better to post a new clarified reply rather than edit an existing post - especially when that post already has replies to it as originally written.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@mrkayaalp wrote:

 I do not have the budget to purchase a development kit. .


Maybe look at 3rd-party modules?

eg, https://www.aliexpress.com/i/32827512831.html - although, of course, the quality can be questionable ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mrkayaalp
Associate III

We solved the problem. We were using a 32.768 MHz instead of 32 MHz oscillator. When we soldered 32 MHz, one SO line pulled logic LOW when CS was asserted.