‎2022-11-11 8:49 AM
Hi everybody.
I 'm trying to make an Si4703 radio module work with an STM32F030K6T6 on STM32CubeIDE.
I have found an example which is made with Coocox, I think. At https://github.com/LonelyWolf/stm32/tree/master/Si4703 but does not it work with STM32CubeIDE.
So, is there some example that works with STM32CubeIDE?
‎2022-11-11 9:17 AM
It looks to use the old SPL for the F1 part.
Expect you'll have to do the porting, seems relatively niche.
The GNU/GCC compiler should be able to do this.
Migrating this into Keil, which has a licence for CM0(+) STM32 parts, should also be possible.
‎2022-11-11 9:27 AM
I 've made a project based on the above mentioned example but I face some issues, e.g.:
void Si4703_Read(void) {
uint8_t i;
uint8_t buffer[32]; // 16 of 16-bit registers
I2C_AcknowledgeConfig(I2C_PORT,ENABLE); // Enable I2C acknowledge
I2C_GenerateSTART(I2C_PORT,ENABLE); // Send START condition
while (!I2C_CheckEvent(I2C_PORT,I2C_EVENT_MASTER_MODE_SELECT)); // Wait for EV5
I2C_Send7bitAddress(I2C_PORT,Si4703_ADDR,I2C_Direction_Receiver); // Send slave address for READ
while (!I2C_CheckEvent(I2C_PORT,I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); // Wait for EV6
// Si4703 read start from r0Ah register
for (i = 0x14; ; i++) {
if (i == 0x20) i = 0x00;
while (!I2C_CheckEvent(I2C_PORT,I2C_EVENT_MASTER_BYTE_RECEIVED)); // Wait for EV7 (Byte received from slave)
buffer[i] = I2C_ReceiveData(I2C_PORT); // Receive byte
if (i == 0x12) break;
}
I2C_AcknowledgeConfig(I2C_PORT,DISABLE); // Disable I2C acknowledgment
I2C_GenerateSTOP(I2C_PORT,ENABLE); // Send STOP condition
while (!I2C_CheckEvent(I2C_PORT,I2C_EVENT_MASTER_BYTE_RECEIVED)); // Wait for EV7 (Byte received from slave)
buffer[i++] = I2C_ReceiveData(I2C_PORT); // Receive last byte
for (i = 0; i < 16; i++) {
Si4703_REGs[i] = (buffer[i<<1] << 8) | buffer[(i<<1)+1];
}
}
In line 'I2C_AcknowledgeConfig' : implicit declaration of function 'I2C_AcknowledgeConfig'.
The same at 'I2C_GenerateSTART'
‎2022-11-11 9:38 AM
STM32F1 SPL functions, you'd need to pull in an instance of that if not part of the project.
http://stm32.kosyak.info/doc/group___i2_c___exported___functions.html
If you're trying to build a HAL F0 project, would suggest constructing a simple shell or donor project for your IC / Board. Then start merging in chunks of the other project, making equivalent functions using the HAL's I2C and UART libraries.
‎2022-11-11 9:47 AM
I 'm trying to build a HAL F0 project.
Thanks, really complicated...I'm lost in the code.. :)
So what I hould do is convert SPL functions to HAL...
‎2022-11-11 10:49 AM
This (taken from here:(
/**
* @brief Enables or disables the specified I2C acknowledge feature.
* @param I2Cx: where x can be 1 or 2 to select the I2C peripheral.
* @param NewState: new state of the I2C Acknowledgement.
* This parameter can be: ENABLE or DISABLE.
* @retval None.
*/
void I2C_AcknowledgeConfig(I2C_TypeDef* I2Cx, FunctionalState NewState)
{
/* Check the parameters */
assert_param(IS_I2C_ALL_PERIPH(I2Cx));
assert_param(IS_FUNCTIONAL_STATE(NewState));
if (NewState != DISABLE)
{
/* Enable the acknowledgement */
I2Cx->CR1 |= CR1_ACK_Set;
}
else
{
/* Disable the acknowledgement */
I2Cx->CR1 &= CR1_ACK_Reset;
}
}
...to HAL?
:o It'll take me a few lifetimes...
‎2022-11-11 11:08 AM
Well presumably you'll want to read the SiLab's data-sheet and understand what's actually needed, at a higher level ,and perhaps use the HAL's HAL_I2C_Mem_Read() and HAL_I2C_Mem_Write() to do register level transactions with a typical I2C methodology.
Register reading example for a uBlox device at I2C address 0x42, read 2 bytes from register 0xFD and 0xFE
uint8_t data[2];
HAL_StatusTypeDef status = HAL_I2C_Mem_Read(&I2CHandle, (0x42 << 1), 0xFD, 1, data, sizeof(data), 100);
If you understand the intent of what's needed you can probably significantly declutter the implementation you're using, and use high level constructs.
‎2022-11-22 3:49 AM
Hi @Panagiotis​ ,
SPL2LL-Converter may be helpful in such case. Look to the documentation for the How To use it.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.