2024-10-27 10:57 PM - edited 2024-10-27 10:59 PM
Hi guys
I need help!
After the installation, I am trying to start a new project in the STM32CudeIDE, it requires a target no more opinions
How can I resolve this?
2024-10-27 11:19 PM
Hello @a-jorge and welcome to the ST Community.
First, you have to go to File>New>STM32 Project. then you can start your project from a MPU/MCU, an evaluation board or an example.
More details are provided on this Wiki
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-28 01:26 AM
Hi,
Is that what I am doing ( File>New>STM32 Project), but the second screen with the list of target select is not snowing up.
I am using ubuntu 24.04
2024-10-28 01:29 AM
Are you using the Last version of CubeIDE (V1.16.1).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-28 01:44 AM
Yes, I am using the Last version of CubeIDE (V1.16.1).
I recorded a small video to show the problem
https://drive.google.com/file/d/1Xh2KV1O5ukZZbHWqwPttRqMuMFU8aegH/view?usp=sharing
2024-10-28 02:13 AM
Infact, this Ubuntu version (V24.04) is not officially supported by STM32CubeIDE. Here is the list of OS supported (in RN):
Supported operating systems and architectures
• Windows® 10 and 11, 64 bits (x64)
• Linux®: Ubuntu® LTS 20.04 and LTS 22.04, and Fedora® 36
• macOS® 12 (Monterey), macOS® 13 (Ventura)
So, I suggest you use on of the OS officially supported.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.