cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE user interface fell apart

foximaxi
Associate

Hi Gents,

Something weird is going on my computer since a long while, but it gets very annoying as I work with more on this computer. If I open a .ioc file, or do anything in STM32CubeIDE that will bring up a non-eclypse dialog, the GUI misbehaves in a very weird way. Best example is if I go to Software Packs -> Select Components menu - it becames absolutely unusable, every time I open it up. I attached a file where you can see, how the window looks like after scrolling the list or open up a dropdown item.

This happens, when e.g.

  • Working with .ioc files, especially its dialogs, but sometimes in the pinout and clock configuration tabs too
  • Select Components dialog

This doesn't happens when e.g.

  • Opening project properties window
  • In the Target Selector

Note, that eclypse dialogs, even if contain "ST elements" like drop-downs, text fields, etc, does not produce this error. If a dialog is fully ST based, this happens.

Also, I tried the followings:

  • Re-install STM32CubeIDE - no resolution
  • Install an older version - no resolution
  • Update Java - no resolution
  • Update graphics card drivers (AMD) - no resolution
  • Replace graphics card -> Intel - this worked, however, the whole system became very unstable...
  • Replace graphics card -> Geforce RTX - no resolution

Further notes:

  • If a dialog is distorted, resizing it will restore the dialog. But every time I interact something, it became distorted again. Continuously resizing helps, but not effective....
  • If two Select Components dialog is opened in two STM32CubeIDEs, the dialog, opened for the last, is working perfectly (please don't tell that hell yeah, this is the solution! 🙄 )

Apparently it has something to do with the graphics card / driver, but I have no idea anymore, how to go further. I use STM32CubeIDE on 3 other computers with no issue.

The configuration I use:

  • Windows 11
  • STM32CubeIDE Version: 1.14.0

Thank you for your support!

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief

Hi,

"The puzzled windows problem" is not really "new" , but afaik until now no solution by STM .

see:

https://community.st.com/t5/stm32cubemx-mcus/cubemx-ui-is-messed-up-again-again-and-again/m-p/580741

 

https://community.st.com/t5/stm32cubemx-mcus/cubemx-interface-bug/m-p/591221#M26001

 

https://community.st.com/t5/stm32cubemx-mcus/cubemx-6-8-1-application-gui-corruption/m-p/568694#M25272

 

...and many more .

Sometimes seems to help, if graphics text or icon size is changed; or using only one screen, if two been used.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
AScha.3
Chief

Hi,

"The puzzled windows problem" is not really "new" , but afaik until now no solution by STM .

see:

https://community.st.com/t5/stm32cubemx-mcus/cubemx-ui-is-messed-up-again-again-and-again/m-p/580741

 

https://community.st.com/t5/stm32cubemx-mcus/cubemx-interface-bug/m-p/591221#M26001

 

https://community.st.com/t5/stm32cubemx-mcus/cubemx-6-8-1-application-gui-corruption/m-p/568694#M25272

 

...and many more .

Sometimes seems to help, if graphics text or icon size is changed; or using only one screen, if two been used.

If you feel a post has answered your question, please click "Accept as Solution".
foximaxi
Associate

Hi,

bad news. I tried to play with text and graphics size, but it just get worse.

Anyway, thank you for your support!