cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE on macOS Catalina: Installing st-stlink-server-1.2.0-3.pkg fails

FAuco
Associate

Hi,

I'm trying to get started with the STM32CubeIDE, but I'm unable to install the required st-stlink-server-1.2.0-3.pkg package (I'm on macOS Catalina). When I try, it fails with the following error message: "This package is incompatible with this version of macOS. The package is trying to install content to the system volume. Contact the software manufacturer for assistance." (see screen capture)

0690X00000ApeIRQAZ.png

So my question is: Is there a revised package coming out soon? Is there anything I can do in the meantime to start using the IDE (e.g. temporarily use an alternative to st-link)?

Thank you for your time and support! A+

Frank

9 REPLIES 9
FMasc
Associate

Same problem here

MSael.960
Associate

I have the same problem as well. I hope the ST team gets on this issue as soon as possible. Thanks.

MGine.806
Associate II

I have posted a topic today in the community asking the same thing.

Do we have a way to solve this problem? Is there any information about a new release package by the ST team?

AKAMA.1
Associate

Same problem.

MGine.806
Associate II

I've open a Case Status with my profile in order to obtain direct assistance from the ST team.

If they provide me a solution (even if temporarily) I'll update this topic

ecode
Associate II

Some problem

运耿.1
Associate

you can find a way to solve the system file right problem( rootless your Mac) and change the file right

mdelgs
Associate

Having the same issue on MacOS in 2022.