2024-08-25 12:10 PM - last edited on 2024-08-25 02:37 PM by Pavel A.
I downloaded and installed the latest STM32Cube IDE. However, I can't compile even the simplest program, because during the creating of a project I get warning stating that I must download and install the Firmware Package.
The system is a Windows 11 virtual machine without Internet access, so I suppose I should download Firmware Package on other computer and then copy to the VM. However, I cannot locate that Firmware Package.
The problem is very similar to this one:
However that solution didn't work for me.
2024-08-25 02:39 PM
Which STM32? How have you tried to locate the firmware package? Can you login from another machine and download the package?