cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE is not connecting to the internet.

ADaxa.1
Associate II

I had several versions of the IDE installed on my machine but none of them could connect to the internet to update or load code. I keep getting the error message "In order to benefit from best experience a network connection is required. Do you want to set connection parameter now?". At first I thought it was because Norton was blocking the the applications through the firewall but I uninstalled Norton and installed the IDE again but that didn't fix the problem. I installed the IDE on my brothers machine which doesn't have Norton and it worked fine on there. I also have used different networks in the past 2 months so that cant be it. Can anyone please help?

10 REPLIES 10

I had the same problem and solved it by changing Active Provider to Direct.

 

Clyde_S_0-1705012346706.png