cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIde hangs during startup after an update

Mat1
Associate III

Hi,

Yesterday I updated my STM32CubeIde. Today it hangs during start.

The message windows do not respond to any actions (see printscreen)

In the log files "E:\work\STM32Cube\.metadata\.ide.log" I have the following entry:

2023-02-01 08:00:55,772 [INFO] Activator:180 - !SESSION log4j initialized
2023-02-01 08:01:20,625 [ERROR] LogOutputStream:74 - [STDERR_REDIRECT] SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder".
2023-02-01 08:01:20,626 [ERROR] LogOutputStream:74 - [STDERR_REDIRECT] SLF4J: Defaulting to no-operation (NOP) logger implementation
2023-02-01 08:01:20,628 [ERROR] LogOutputStream:74 - [STDERR_REDIRECT] SLF4J: See http://www.slf4j.org/codes.html#StaticLoggerBinder for further details.
2023-02-01 08:11:04,816 [INFO] Activator:179 - 

Thanks for any ideas.

0693W00000Y9ghBQAR.png

4 REPLIES 4
Mat1
Associate III

Creating a new workspace has worked for me.

Semer CHERNI
ST Employee

Hello @Matthias Stähli​ 

First let me thank you for posting.

Could you provide the complete log file both the ".ide.log" and the ".log"

Thanks and kind regards,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.