2023-09-22 05:21 AM - edited 2023-09-22 05:22 AM
Hi,
after installing STM32CubeIDE v1.11, I get the following error when running Help-->Check for updates
I've already tried the hints from other posts like clearing the cache, checking proxy, checking the https addresses, etc.
Other updates work, like Help-->Check for Target Selector Device Database Updates.
I've also uninstalled STM32CubeIDE completely and freshly installed v1.13 but the behavior remains.
Any help would be appreciated.
Regards,
Peter
2023-09-22 05:29 AM - edited 2023-09-25 11:23 PM
Just for info: the new v1.13 is (otherwise) working fine?
2023-09-25 10:24 AM
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2023-09-26 06:48 AM - edited 2023-09-26 06:52 AM
Hello @PowerStation ,
At first, could you try to check the proxy settings following these steps:
- Under Window --> Preferences--> Network Connections, activate Native provider
- Under Window --> Preferences--> Firmware Updater, click on Check Connection
don't forget Apply and Close, if the connection works.
Also, reload OpenSTLinux Releases under preferences-->available software sites, as shown in this screenshot
Thanks,
Rim.
2023-09-26 07:50 AM
Hello Rim,
Native provider was activates but I cannot find "Window --> Preferences--> Firmware Updater, Check Connection"
Reloading OpenSTLinux Releases results in the same error message:
Thank you.
Regards, Peter