cancel
Showing results for 
Search instead for 
Did you mean: 

Reserving microcontroller Flash non-volatile memory

JimEno
Associate III

I want to reserve a chunk of internal Flash memory in the micro-controller to store some user parameters. I want to develop a custom driver to manage the sector of Flash including erasing and re-writing the sector (there better be utility functions for Flash Sector erase and write). In the 'olden days' with a linker command file, I could do that easily. I can't seem to find that capability in the STMCube IDE with the file <project.ioc>. How do I do this?

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

The linker script will be a *.ld file that is created when you generate the code. You can modify the main FLASH section within the linker script to avoid writing to the reserved flash sector.

If you feel a post has answered your question, please click "Accept as Solution".