2020-10-18 11:09 PM
Cube IDE started to lock on starting this morning. Progress bar moves to approximately 60% then stops there. Is that a general problem? I have removed and re installed it( Version 1.4.2), but result is same. When I return to CubeIDE V1.3.0 there is no problem. But I have problems with mismatch with my projects generated under v1.4.2.
Update : Resolved. That was a problem due to corrupted workspace settings. Thanks to ones who paid attention.
Kind Regards.
2020-10-20 06:13 AM
Sorry that I'm late to the thread. I'm glad to hear that you managed to figure it out.
Could you reproduce the issue again if you wanted to? If so, I would be happy to take a look at it. Seems like CubeIDE should handle an error like this in a better way than just stopping at a progress bar.
2020-10-20 08:47 AM
2021-06-17 04:48 AM
Exactly the same issue out of nowhere. I have been using cubeIDE for a while, now decided to run it again and same as you - cubeIDE loads to 60-70% and freezes.
What exactly is the cause of this issue? Do i have to delete the corrupted workspace?