2019-05-01 08:34 AM
I'm sure it's something silly and I can't believe I'm the only person who has seen this message but searching this site doesn't yield any clues. Can someone point me to what I am setting up wrong, presumably in the Debug Configuration menu ?
2020-01-05 10:59 AM
I installed STM32CubeIDE and also get the
Error with command: gdb --version
Cannot run program "gdb": Launching failed
message. Perhaps an explanation of how to install gdb and set up STM32CubeIDE to use it would be usefull. Documentation is usefull.
2020-01-05 12:43 PM
UM2563 STM32CubeIDE installation guide ?
All external tools are installed during STM32CubeIde install in the plugins folder. On a recent Win10 install, compiler+debugger are in C:\ST\STM32CubeIDE_1.1.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610.
Avoid complications in the install path: no spaces, no long path, all ASCII.
2020-01-05 12:49 PM
Hello - I was going to come back here and update. I went to Debug Configurations, and changes Debugger from gdb to arm-none-eabi-gdb, enabled Serial Wirer Viewer. That got me running. Just now commented out the " __HAL_AFIO_REMAP_SWJ_DISABLE()" call. I am running what I believe to be commonly known as the Blue Pill STM32F103C8 board. I am running my code now ..... thank you for making STM32CubeIDE available to hobbyists such as myself !
2020-01-05 02:33 PM
I changed GDB debugger from gdb to arm-none-eabi-gdb, and enabled Serial Wirer Viewer. Thank you.
2020-01-20 04:52 AM
After working a view days i experienced the gdb --version error this afternoon too. Deleting a debug/prjname.elf file in Debug Configuration // C/C++ Application solved the problem for me.
2020-01-26 11:56 AM
Same problem!
I just installed STM32CubeIDE (Windows 10) and tried to blink an LED on a brand new Nucleo-64 board STM32F303RE.
You know, a simple test to make sure everything is working right. Ha well, funny thing is... it's not working.
I selected the Nucleo-F303RE board in the CubeMX configuration and followed the CubeIDE getting started video on youtube.
Everything is great until I click 'Debug'. That's when I get the "Error with command: gdb --version" message.
How do we fix this???
What I've tried:
In the Debug settings tab I changed "gdb" to point to the location of "ST-LINK-gdb-server.exe" that I found after searching for GDB in the CubeIDE install folder. But that didn't work.
I haven't found anything in the STM32CubeIDE install guide that says I need to install something else or change the debug configuration.
A help is greatly appreciated!
Thanks!
2020-01-26 12:41 PM
It seemes I stumbled on a solution.
I went back and selected Project->Build Project
Then Run->Debug As->STM32 MCU C/C++ Application
A new window popped up asking me to make a new debug configuration. I selected 'Okay' without changing anything.
Then the IDE asked if I wanted to open the debug perspective and I selected 'Switch'.
Now debugging is active and stopped at the first line in my program waiting for me to proceed. 🙂
I think the problem was I had previously selected the wrong build option instead of 'Build Project'.
I hope this helps!
2020-01-29 09:29 PM
I have the same issue too.
A month ago, I used NUCLEO to test some function and the program progress work success.
But few days ago, STM32CubeIDE suddenly can not execute program and pop-out the message below, and I have no idea how to solve this problem.
Error with command: gdb --version
Cannot run program "gdb": Launching failed
2020-01-29 10:57 PM
> Error with command: gdb --version
> Cannot run program "gdb": Launching failed
This is testing for presence of the debugger. The error message should read "debugger not found"
Be sure that your project/Debug Configuration is of type STM32 Cortex-M...
For every Debug configuration, there is a .launch file. Open it with a text editor. There is a line:
<stringAttribute key="org.eclipse.cdt.dsf.gdb.DEBUG_NAME" value="${TOOLCHAIN_PATH}/arm-none-eabi-gdb"/>
Check that path.
You can edit the path to be the absolute path for the debugger.
On my Win10 PC it is
<stringAttribute key="org.eclipse.cdt.dsf.gdb.DEBUG_NAME" value="C:/ST/STM32CubeIDE_1.1.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610/tools/bin/arm-none-eabi-gdb"/>
your mileage may vary.
Avoid complications in the path like space char's umlauts, etc.
Note: Couldn't figure out how to set/change ${TOOLCHAIN_PATH} in the GUI.
2020-01-30 12:04 AM
I found the problem.
If you run the debug, you should check your debug configuration and use "STM32 Cortex-M C/C++ Application".