cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.5.0 released

mattias norlander
ST Employee

STM32CubeIDE 1.5.0 released

STM32CubeIDE 1.5.0 was released this week on st.com as well as a in-tool update patch.

Caution: The in-tool update does not allow updating drivers and ST-LINK server tool. Full installer is required for this.

What is new in 1.5.0? (only some highlights)

  • Target support updated in-sync with STM32Cube ecosystem in general. In particular :
    • Added the support for the STM32WL Series
    • Extended the support for the STM32G0 Series to the new STM32G0Bxxx and STM32G0Cxxx devices
  • Integration of STM32CubeMX 6.1.0, STM32CubeProgrammer 2.6.0 and latest versions of various other STM32 deliverables.
  • New features :
    • Added FreeRTOSâ„¢ debug support
    • Added toolchain manager
      • Allows optional installation of new Arm and Gnu Tools for STM32 toolchains based on GCC 9-2020-q2​
      • Reduces STM32CubeIDE installer packages by only bundling one toolchain: Gnu Tools for STM32 based on 7-2018-q2
    • Improved OpenOCD supporting :
      • Live expressions
      • Serial Wire Viewer (SWV)
    • Added the ability to write values while target is running in the Live Expression view
    • Extended the SFRs view with Arm® core registers
    • Added Ubuntu® 20.04 support
    • For MPU series :
      • Updated to OpenSTLinux 2.1

Main issues fixed in STM32CubeIDE 1.5.0

Only a sub-set of the many tickets closed are mentioned in the release note.

Known problems and limitations

Please refer to the release note.

Where do I Obtain CubeIDE 1.5.0?

4 REPLIES 4
this_is_a_username
Associate

Where can I find this version, the download tool does not provide this version.

select 1.15 on the drop-down menù here https://www.st.com/en/development-tools/stm32cubeide.html

I am looking for 1.5.0 not 1.15, the link you provided does not provide 1.5.0. Is there a separate file server I can download it from?

sorry, misread. It seems availble only on the Japanese site https://www.stmcu.jp/design/sw_dev/pc_soft/66469/