cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.19.0 Problem migrating OCTOSPI2 (STM32H730) from 1.18.1

MHoll.2
Senior III

I have a ioc file created with Version 1.18.1, that enables only the OCTOSPI2 (and some RCC and clock settings).

Importing this file (see attachmend) the OCTOSPI2 gets disabled, further more it is non longer possibile to re-enable it as QUAD-SPI!

MHoll2_0-1751961259995.png

If added with out migration the IOC it is working as before.

10 REPLIES 10

The problem seems to be resolved in STM32CubeMX 6.16.0 (together with STM32CubeIDE 2.0.2).