2025-03-16 6:54 PM
I had the latest version of 1.16 installed. I upgraded that installation to 1.18 which was just released. When I double click the ioc file it asks if I want to continue or to migrate. When I choose migrate it doesn't work. It freezes and I have to close the IDE and restart it. After fighting with this for a day, I downloaded 1.18 and installed it in a separate directory. This installation had no problem migrating. I attached the eclipse log file.
2025-03-17 8:19 AM
Hello @Carl_G
First let me thank you for posting.
Could you share the ioc file.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-18 4:32 AM