cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE 1.17.0 released

Semer CHERNI
ST Employee

We are pleased to announce to you that the release 1.17.0 of STM32CubeIDE is available.

What is new in 1.17.0:

  • Microcontrollers, microprocessors, and board lists aligned with STM32CubeMX:
    • Added the support for the STM32N6 series
    • Added the support for the STM32U3 series.
    • Added the support for the STM32WL3x line
    • Added the support for the STM32MP23xx microprocessors
    • Added the support for the STM32MP25xx microprocessors in a TFBGA361 16 mm × 16 mm package
    • Added the support for new microcontrollers in the STM32C0 series and related Nucleo boards (NUCLEO-C051C8 and NUCLEO-C092RC)
    • Added the support for new microcontrollers in the STM32G4 series
    • Added the support for new microcontrollers in the STM32WBA series and the related B-WBA5M-WPAN board
  • Simplified user authentication interface
  • Added support for debug authentication with password for the STM32N6 series.
  • Improved support of OpenSTLinux plugin to be version agnostic
  • Enabled the installation of both STM32MP1 and STM32MP2 flavors of OpenSTLinux plugins within the same STM32CubeIDE instance.
  • Added support for flashing the .bin file during debugging.

Main fixed issues in 1.17.0:

Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata

Known problems and limitations in 1.17.0:

Refer to the STM32 microcontroller wiki at:
wiki.st.com/stm32mcu/wiki/Category:STM32CubeIDE_errata

How to get STM32CubeIDE 1.17.0:

  • Under this link
  • Or update your current installation of STM32CubeIDE using: Help > Check for updates (The in-tool update does not allow updating the drivers and ST-LINK server tool. Full installation is required for this to be done).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

12 REPLIES 12

If you want guarantees of support, you probably need to be looking to paid-for commercial offerings ...

dirtcooker
Associate

myST -> Login does not work properly on Linux Mint (ubuntu 22 based). I needed to work on some stm32 code pronto today, have a new machine so naturally I downloaded the latest and installed it. Big mistake. It forced me to login repeatedly then promptly forgot, went to myST -> Login and entered my account, then tried to download packages from Help | Manage Embedded Software without luck. cube finder was unable to download the packages too. Finally, I uninstalled 1.17 then reinstalled 1.12. Fortunately, I had a copy of the installer, since it is gone from st.com

Please get rid of this login ***. I have wasted hours. I will not recommend stm32 for future projects if this *** continues. It's prob too late to change for this project, but fortunately 1.12 still works OK

jalks
Associate II

Loving the expanded support for STM32 series and the new microcontrollers. This will definitely make development smoother. Excited to try the new features in 1.17.0! :rocket: