cancel
Showing results for 
Search instead for 
Did you mean: 

STM32cubeide 1.13.2 & cubeMX integrated

Fendo59
Associate III

I installed STM32CubeIDE 1.13.2 in the hope that the problem of the 1.13.1 release has been solved (see My old topic ) . Nothing the problem continues to exist. To make the integrated CubeMX work I have to open and close the IDE 3 or 4 times, also if it doesn't start I have to delete the home/user/workspace_1.13.2/.metadata directory. (for my system config see My old topic )

Thanks for your help.
Ferdinando

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Hi!

Are there any news.
I installed the debian package Stm32CubeIDE 1.15.0 but the problem remained the same if not worse.
I tried to install the Linux Generic 1.15.1 version and modified the stmcudeide_wayland file, with sudo privileges, by adding the line "export GTK_THEME=Adwaita" after the line "export GDK_BACKEND=x11".
Now it work at 95%, occasionally it still crashes, but just close and relaunch the program.
You no longer need to delete any files.

However, I hope for further improvement.