2023-07-10 8:44 AM
STM32CubeIDE 1.13.0 was released today on st.com as well as an in-tool update patch.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-19 12:15 AM - edited 2023-07-19 12:16 AM
After installing STM32CubeIDE 1.13.0 I have no menu bar any further. I tried to configure menu bar visibility for perspectives, which had no effect. I also tried to reinstall STM32CubeIDE 1.13.0 but still no menu bar.
I am running windows 11 and having STM32CubeIDE 1.12.1 and 1.13.0 installed in two separate folders.
best regards
PScal
2023-07-28 6:33 AM - edited 2023-07-28 6:34 AM
I always had issues when upgrading.
Best way is to uninstall the current IDE and install the new one.
If still having issues, delete the .metadata folder in the workspace.
2023-07-28 11:16 AM
Upgrading on a macOS box just works. Downgrading was easy too, just get time machine to take it back to before the update.
I find it weird that after 40 years, Microsoft still treats backups as second class citizens.