cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32

M_J
Associate II

How to use timer interrupt in GPIO interrupt

8 REPLIES 8
MM..1
Chief III

Priority?

M_J
Associate II

Timer 

AScha.3
Chief III

Why ?

If you feel a post has answered your question, please click "Accept as Solution".
MM..1
Chief III

primary your personal sended code nobody see then nobody help.

volatile uint8_t count = 0;
			HAL_GPIO_TogglePin(GPIOB, Red_Led_Pin);
			HAL_Delay(100);

For ISR variables need volatile. Your count++ and if else is litle complicated. 

And your code isnt timer interrupt in GPIO. You only start timer with IT method aplied...

HAL_TIM_Base_Start_IT(&htim3);

And use Delay in callback is mistake if systick isnt higher priority code hang here

 

M_J
Associate II
/**
  * @brief GPIO Initialization Function
  * @param None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOH_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOB, Green_Led_Pin|Red_Led_Pin, GPIO_PIN_RESET);

  /*Configure GPIO pin : Push_Button_Pin */
  GPIO_InitStruct.Pin = Push_Button_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(Push_Button_GPIO_Port, &GPIO_InitStruct);

  /*Configure GPIO pins : Green_Led_Pin Red_Led_Pin */
  GPIO_InitStruct.Pin = Green_Led_Pin|Red_Led_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  /* EXTI interrupt init*/
  HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
M_J
Associate II

If I press the user button for 2 sec.  Then red led will tern on .... Again I press button then red led will tern off.....If I continue press the button led will be tern off........ 

I did some changes but my problem is not solved ...

 

LCE
Principal

Dude, tell the people what you want to achieve.

Even your starting post "How to use timer interrupt in GPIO interrupt" is ridiculous, we have no time for guessing.

M_J
Associate II

Extremely  Sorry ... next time definitely I will try