cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 I2c won't send data

fontys_student
Associate II

I am trying to get to use I2C on my stm32L4R5ZIT-P.

i am trying to configure a sensor by sending data but the I2C pins wont give a signal?

i dont ude interups or DMA

these are the pins that i use and the setting for I2C:

fontys_student_2-1705416583285.png

 

fontys_student_1-1705416526079.png

this are the includes i use

fontys_student_3-1705416909107.png

this is my code. i don't have any errors or warnings in the code

fontys_student_4-1705416964693.png

how do i fix it and make shure i can send data out?

 

7 REPLIES 7
TDK
Super User

Does HAL_I2C_IsDeviceReady return HAL_OK? Do your other functions return HAL_OK?

If you feel a post has answered your question, please click "Accept as Solution".
Bob S
Principal

What do you mean "won't give a signal"?  Are you looking at the SDA and SCL lines with a scope or logic analyzer?

"I don't have any errors or warnings in the code" -> means no compiler errors or warning.  You need to check the return values from the HAL calls. Do you call MX_I2C2_Init() somewhere before the code you posted?

Is this a custom board or one of the ST Nucleo (or Disco?) boards?  Are there external pull-up resistors on the SCL/SDA lines?  Using only the STM32's internal pull-ups MAY work for testing but should not be relied on in a production device - they are too high a resistance.

Also, when posting code, please don't post images, copy/paste the code into the forum message using the code tags (click on the "..." button then "</>").

i am new to the stm platform. where can i see if the functions give a HAL_OK


@fontys_student wrote:

 where can i see if the functions give a HAL_OK


It will be the return value from the function call; eg, 

HAL_StatusTypeDef result; // for the return value from HAL function calls result = HAL_I2C_IsDeviceReady( &hi2c2, 0x40<<1, 10, 1000 );

 

BTW: rather than writing `0x40<<1` as a Magic Number, it would be better style to give it a meaningful name; eg,

#define SENSOR_I2C_ADDRESS (0x40<<1)

then you can write:

 

result = HAL_I2C_IsDeviceReady( &hi2c2, SENSOR_I2C_ADDRESS, 10, 1000 );

 

Which is not only clearer & easier to understand, but also easier to maintain; eg, if you find that the address needs changing...

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User

UM1884 - Description of STM32L4/L4+ HAL and low-layer drivers:

https://www.st.com/resource/en/user_manual/um1884-description-of-stm32l4l4-hal-and-lowlayer-drivers-stmicroelectronics.pdf

See also https://www.st.com/en/microcontrollers-microprocessors/stm32l4r5zi.html#documentation for further documentation - Application Notes, etc ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

when i try do this i get a HAL_busy back

this is my full code. i use the internal pullup of the stm 32

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "stm32L4xx_hal_i2c.h" #include <string.h> #include <stdio.h> /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ I2C_HandleTypeDef hi2c2; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_I2C2_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_I2C2_Init(); /* USER CODE BEGIN 2 */ if (HAL_I2C_EnableListen_IT(&hi2c2) != HAL_OK) { Error_Handler(); } /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ //configuration reset while (1) { HAL_StatusTypeDef result; // for the return value from HAL function calls result = HAL_I2C_IsDeviceReady( &hi2c2, 0x40<<1, 10, 1000 ); /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ uint8_t confReset[2]; confReset[0] = 0x80; confReset[1] = 0x00; uint8_t conf; conf = 0x00; uint8_t confVal[2]; confVal[0] = 0x39; confVal[1] = 0x9F; uint8_t cal; cal = 0x05; uint8_t calVal[2]; calVal[0] = 0x57; calVal[1] = 0x62; /* Infinite loop */ /* USER CODE BEGIN WHILE */ //configuration reset HAL_I2C_Master_Transmit(&hi2c2, 0x40<<1, confReset, 2, 10); //configuration setup HAL_I2C_Mem_Write (&hi2c2, 0x40<<1, conf, 1, confVal, 2, 10); HAL_I2C_Mem_Write (&hi2c2, 0x40<<1, cal, 1, calVal, 2, 10); // HAL_I2C_Mem Write (hi2c, (0x40<<1), 32768, 16, addata, Size, Timeout); // HAL I2C_Mem Read (hi2c, DevAddress, MemAddress, MemAddSize, pData, Size, Timeout); /* USER CODE END WHILE */ /* USER CODE END 3 */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) { Error_Handler(); } /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 16; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV4; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK) { Error_Handler(); } } /** * @brief I2C2 Initialization Function * @PAram None * @retval None */ static void MX_I2C2_Init(void) { /* USER CODE BEGIN I2C2_Init 0 */ /* USER CODE END I2C2_Init 0 */ /* USER CODE BEGIN I2C2_Init 1 */ /* USER CODE END I2C2_Init 1 */ hi2c2.Instance = I2C2; hi2c2.Init.Timing = 0x10707DBC; hi2c2.Init.OwnAddress1 = 0; hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c2.Init.OwnAddress2 = 0; hi2c2.Init.OwnAddress2Masks = I2C_OA2_NOMASK; hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; if (HAL_I2C_Init(&hi2c2) != HAL_OK) { Error_Handler(); } /** Configure Analogue filter */ if (HAL_I2CEx_ConfigAnalogFilter(&hi2c2, I2C_ANALOGFILTER_ENABLE) != HAL_OK) { Error_Handler(); } /** Configure Digital filter */ if (HAL_I2CEx_ConfigDigitalFilter(&hi2c2, 0) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN I2C2_Init 2 */ /* USER CODE END I2C2_Init 2 */ } /** * @brief GPIO Initialization Function * @PAram None * @retval None */ static void MX_GPIO_Init(void) { /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOF_CLK_ENABLE(); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

 

 

TDK
Super User

Start with blocking functions. Call HAL_I2C_IsDeviceReady and ensure it returns HAL_OK before calling any other I2C function. Don't call HAL_I2C_EnableListen_IT at the start.

If you feel a post has answered your question, please click "Accept as Solution".