2021-01-08 03:50 AM
Hello there...
Hope, all are doing well
I was working with the former version 1.4.0 on the top of it, i have made my project
After updating the version 1.5.1, i'm unable to build the project any more
Not only that but, I'm unable to clean the project!!!
Here is the error logs
Can any one help me here
Thanks!
2021-01-08 07:02 AM
I would try to reinstall CubeIDE and/or reboot.
2021-01-11 12:22 AM
okay, is there anything that i can do except re-install ?
Thanks
2021-01-26 11:36 PM
Solve after re-installing
Thanks :)