cancel
Showing results for 
Search instead for 
Did you mean: 

St-Link is not detected MacOS 15.3.1

MA4
Associate III

Hello,

I update my computer to MacOs 15.3.1 and I have a similar problem to when MacOs 15 arrived. The St-Link (ST-Link v3 mini) is not detected with Cube IDE (CubeIDE v. 1.17.0).
It worked fine in MacOS 15.1.1

I've tried starting the IDE as admin and adding the link's path to the path list, but it doesn't work. (https://community.st.com/t5/stm32cubeide-mcus/stlink-server-with-macos-15/td-p/705089)


On the other hand, it is well detected with STM32Programmer.

I added the IDE to the development tools in the security tab of the computer settings, just in case the problem came from the fact that apple could have changed the security rules, but that didn't solve the problem.

 

2 REPLIES 2
Souhaib MAZHOUD
ST Employee

Hello @MA4 


Could you please take a look at this FAQ . The workarounds could be a solution to your problem.

 

BR,

Souhaib

MA4
Associate III

Hello,

Thank you for our answer.

I'm not sure if it's USB related cause it was working before I updated my OS. It also works with STM32Programmer, I only have the issue with STM32CubeIDE