cancel
Showing results for 
Search instead for 
Did you mean: 

ST_LIK Failed to bind to port 61235, error code -1 No such file or directory

PZamb.2
Associate III

Hi

I upgrade stmcubeide  from 1.12.1 to 1.13.2, after the st-link not work in debugger , i view the followed error:

Failed to bind to port 61235, error code -1: No such file or directory
Failure starting SWV server on TCP port: 61235
Failed to bind to port 61234, error code -1: No such file or directory
Failure starting GDB server: TCP port 61234 not available.
Shutting down...
Exit.

In the previous version the ST-LINK work , what is happend?

I tried with STM32CubeProgrammer to connect to board and programming , work fine.

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Mahmoud Ben Romdhane
ST Employee

Hello @PZamb.2 ,

First let me thank you for posting.

I suggest that you consult this link:  Solved: Re: No ST-Link detected - Only in CubeIDE 1.13.2.

Thanks. 

Mahmoud.

View solution in original post

4 REPLIES 4
Mahmoud Ben Romdhane
ST Employee

Hello @PZamb.2 ,

First let me thank you for posting.

I suggest that you consult this link:  Solved: Re: No ST-Link detected - Only in CubeIDE 1.13.2.

Thanks. 

Mahmoud.

Hi thank for your answer, I reboot the pc and now work

 

PZamb.2
Associate III

Hi

now have the same problem again:

Failed to bind to port 61236, error code -1: No such file or directory
Failure starting SWV server on TCP port: 61236
Failed to bind to port 61235, error code -1: No such file or directory
Failure starting GDB server: TCP port 61235 not available.
Shutting down...

I try to replace ST-link server from 2.1.1 to 2.1.o, like suggest from post , but no effect.

The  ST-Link works with stm programmer but not work in stm32cubeide 1.13.2 (windows 11).

now reboot of PC don't have effect.

someone have any suggest ?

 

 

I had exactly same issue with STM32CubeIDE version 1.15.1. Had a NUCLEO-G474RE run over night, then i unplugged to do some work. After replugging the usb cable the debugger no longer worked, and i got the error message:

Failed to bind to port 61236, error code -1: No such file or directory
Failure starting SWV server on TCP port: 61236
Failed to bind to port 61235, error code -1: No such file or directory
Failure starting GDB server: TCP port 61235 not available.
Shutting down...

If i used the STM32CubeProgrammer, then i could connect, program and read the SWD debugging info fine. So the problem must be with the IDE. After some searching around i found a patch that worked for me. The STLink usb driver had to be reinstalled, by running STM32CubeIDE->drivers->STLinkUSBDriver:dpinst_x86.exe(This depends on your CPU). Afterwards the debugger worked again!