cancel
Showing results for 
Search instead for 
Did you mean: 

Set up External Memory in STM32CUBEIDE

Minti
Associate II

Hi,

i try to switch my working IDE from Atolic Truestudio to STM32CUBEIDE.

A fraction of my code is executed on an external SDRAM.

With Truestudio this works, when i initialize the SDRAM in a Startup Skript.

I did't find the same feature in STM32CUBEIDE.

How do i set up external Memory in the STM32IDE?

Without the external SDRAM my Projekt runs as intended.

My Setup: STM32F767NI

Segger J-Link plus

STM32CUBEIDE 1.5.0

Thank u in advance :)

0 REPLIES 0