2025-02-16 10:21 AM
Hi.
I am using TouchGFX and it works fine,
My MCU is STM32H743
But when I use the SDRAM for other things the code does not work.
My question is:
Can I use struct in the SDRAM.?
I have this one in my c file.
SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
In my h file as follows:
typedef struct {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
}SD_CARD;
extern SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
My Linker file is as follows:
/* Entry Point */
ENTRY(Reset_Handler)
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM_D1) + LENGTH(RAM_D1); /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x400; /* required amount of heap */
_Min_Stack_Size = 0x800; /* required amount of stack */
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 16M
SDRAM (xrw) : ORIGIN = 0xC0000000, LENGTH = 32M
}
etc
etc
etc
.ARM.attributes 0 : { *(.ARM.attributes) }
BufferSection (NOLOAD) :
{
*(Video_RGB_Buffer Video_RGB_Buffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
*(TouchGFX_Framebuffer TouchGFX_Framebuffer.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >SDRAM
SDCardSection (NOLOAD) :
{
*(SDCardSection SDCardSection .*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >SDRAM
Best Regards.
Solved! Go to Solution.
2025-02-17 7:03 AM
Hello,
You've already declared and relocated it in SDRAM in the c file:
SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
No need to relocate it again in the header file:
typedef struct {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
}SD_CARD;
extern SD_CARD SdCard;
The linker knows by the key "extern" it's the same variable you've declared in .c file.
2025-02-17 6:25 AM
Hello @Hector_R and welcome to the community!
I do not see why you could not use a struct in the SDRAM.
I do not think you need
extern SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
in your header file. Just declare the type in the source file.
Are you able to use your SDRAM when you don't use the structure?
Regards,
2025-02-17 7:03 AM
Hello,
You've already declared and relocated it in SDRAM in the c file:
SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
No need to relocate it again in the header file:
typedef struct {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
}SD_CARD;
extern SD_CARD SdCard;
The linker knows by the key "extern" it's the same variable you've declared in .c file.
2025-02-17 7:25 AM
Hello Gaetan.
I need to add the structure as an extern because those variables are used in other files. (from TouchGFX)
This works well.
My .c file.
// My structure
SD_CARD SdCard
In my .h file
typedef struct {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
}SD_CARD;
extern SD_CARD SdCard;
As you can see when
But I would use the SDRAM because I need to add big buffers to display files (SD CARD file names)
But this way the display does not work.
typedef struct {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
}SD_CARD;
extern SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
2025-02-17 7:28 AM
As I said you need to declare and relocate that structure in the c file:
SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
Then export it the header file without any relocation:
typedef struct {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
}SD_CARD;
extern SD_CARD SdCard;
2025-02-17 7:40 AM
Hello Friend!.
Yes, I have tested it right now.
But the problem is still there.
If I use a simple buffer it works, for example:
.c file
char SdCard_Name[256] __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
extern SdCard_Name[256];
2025-02-17 7:43 AM
You need to specify what do you mean by "it doesn't work". Struct wrongly filled with incorrect values? not accessible? or what?
2025-02-17 8:00 AM
Hello.
I have done a debug.
When the first MX_TouchGFX_Process(); is called all is corrupted.
MX_GPIO_Init();
MX_DMA_Init();
MX_QUADSPI_Init();
MX_FMC_Init();
MX_CRC_Init();
MX_LTDC_Init();
MX_DMA2D_Init();
MX_TIM2_Init();
MX_SDMMC1_SD_Init();
MX_FATFS_Init();
MX_I2S1_Init();
MX_USART1_UART_Init();
MX_I2C1_Init();
MX_USB_HOST_Init();
MX_TouchGFX_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
MX_TouchGFX_Process();
/* USER CODE BEGIN 3 */
}
I am not using FreeRTOS.
This image shows the display.
2025-02-24 2:27 AM
Hello @Hector_R ,
Perhaps you can try to set the alignment in the structure definition directly:
typedef struct __attribute__((aligned(4))) {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
} SD_CARD;
extern SD_CARD SdCard;
If that doesn't work, you can try to disable the cache.
Regards,
2025-02-24 7:43 PM
Hi.
Thanks for your help.
I have found that the problem comes when I use my variable in a TouchGFX file.
For example:
I have my struct in my C file.
SD_CARD SdCard __attribute__((section("\"SDCardSection\""))) __attribute__((aligned(4)));
and my h file
typedef struct {
char Name[256];
char Path[1000];
char File[2000];
uint8_t LogicalDrive;
}SD_CARD;
extern SD_CARD SdCard;
At this point, all compiles are ok.
But when I use my variable in a TouchGFX function all collapses.
I can compile all well without errors.
void CustomContainer2_1::UpdateText(uint16_t value)
{
char*p;
p = SdCard.File;
...
...
...
}
Thanks all for your help.
I going to continue looking for a solution.