cancel
Showing results for 
Search instead for 
Did you mean: 

Sample FreeRTOS TCP/IP projects that run on the NUCLEO-F4xx dev boards.

NMali.1
Associate

I'm new to FreeRTOS and STM32F4xx processors and therefore looking for some Sample FreeRTOS TCP/IP projects to aid my learning.

Regards

Nasir

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ms1802
Associate II

There are many examples in the STM32Cube_FW_F4_xx libraries (when you install the Cube libraries)

most of the stuff using TCP/IP uses FreeRTOS as it make life easier.

I assume you have an F4 ir F7 with a built in PHY and Ethernet socket - nearly all the examples use this, rather than bolt on modules.

(install Agent Ransack - fantastic search tool - and look for key words like tcp FreeRTOS )

eg

STM32Cube_FW_F4_V1.24.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_UDP_Echo_Server

STM32Cube_FW_F4_V1.24.0\Projects\STM324x9I_EVAL\Applications\LwIP\LwIP_UDPTCP_Echo_Server_Netconn_RTOS

They may not be specific to your F4, but its never hard to convert from one to another.

Try Creating a CubeMX project with FreeRTOS and TCP/IP enables, then look at the examples and copy the relevent code in.

Pay partucular attention to the FreeRTOSConfig and lwipopts.h config headers - get these wrong an things will nvever work properly.

Have fun!