2020-04-10 4:52 AM
Hi All,
I'm using Nucle0-F429ZI board with SMT32Cube IDE. I can't debug after deleting sector 23. However, after the sector 12 deletes , there is no problem.
I get the error when I press the debug button again after running the code below.
//Erasing sector23
HAL_FLASH_Unlock();
EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
EraseInitStruct.VoltageRange = VOLTAGE_RANGE_3;
EraseInitStruct.NbSectors = 1;
EraseInitStruct.Sector = FLASH_SECTOR_23;
status = HAL_FLASHEx_Erase(&EraseInitStruct, &SECTORError);
HAL_FLASH_Lock();
Error is:
Error in final launch sequence:
Failed to execute MI command:
load C:\\Users\\think2\\STM32CubeIDE\\workspace_1.3.0\\AppBoot\\Debug\\AppBoot.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\think2\\STM32CubeIDE\\workspace_1.3.0\\AppBoot\\Debug\\AppBoot.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\think2\\STM32CubeIDE\\workspace_1.3.0\\AppBoot\\Debug\\AppBoot.elf
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation
What is the reason of this?