cancel
Showing results for 
Search instead for 
Did you mean: 

"Breakpoint installation failed: unmatched quote" at CubeIDE

Fèlix
Associate II

Hi,

I’ve a problem trying to setup breakpoints. At any code line where I try to setup a breakpoint, it does not matter which, neither if it’s the main.c or a library, it just keeps telling me “Breakpoint installation failed: unmatched quote�? as you can see in the attached image :\

Actually I’m using Nucleo-F429. I would appreciate if someone can have a clue about why is like that.

Thanks, 

2 REPLIES 2
Markus GIRDLAND
ST Employee

I'm clicking around in a newly generated Nucleo-F429 project and I can't seem to get the same problem.

Any special procedure to recreate the issue?

Any change if you switch to a fresh workspace?

Fèlix
Associate II

Changing the workspace solved the problem.

Thanks!